Handles, Pulls, and Knobs Hardware Basics

Handles and knobs are used for a wide range of applications, such as doors, drawers and machinery.
This section introduces the basics about them, what types there are, and how to choose the right product for your purpose.

What are handles, pulls, and knobs?

Pulls, handles, and knobs are the parts you hold to open or close doors and drawers on furniture or machinery.
In the next sections, we'll show you their appearance (material and finishing), explain how to install them, and provide tips for choosing the right product.

Types of Handles, Pulls, and Knobs

For Furniture

For furniture, handles, pulls, and knobs are mounted on only one side of the furniture because they are opened only from the outside.
Conversely, for interior doors, handles are often mounted to both the inside and outside.
In addition, sizes for furniture are smaller than those for interior doors.

Back Screw Mount Handles

Read More

Back screw mount handles are mounted with screws from the back of a drawer and cabinet.
By using them, you can give your furniture a seamless and elegant finish, as the screws will not be visible from the front.

Video: The difference between a back screw mount handle and a surface mount handle

Front Screw Mount Handles

Read More

Front screw mount handles are mounted from the front.
They are easy to position and mount. They are recommended when mounting from the back is not possible (there is no space in the back) or when you need to mount a handle to a place that is hard to reach.

Video: The difference between a back mount handle and a surface mount handle

Knobs

Read More

While handles are operated with a grip, knobs are often smaller and are operated with a pinching action with fingers.
For knobs with a specific directional orientation, like the ones shown below, sometimes have a rotation stopper in order to keep in the right position and direction.

Rotation Stopper

Recessed Pulls

Read More

Recessed pulls are embedded into doors and drawers so that they do not stick out.
Recessed pulls can be classified into two types based on the presence or absence of a "handle lip," which is a raised edge around the opening of the handle that helps to grip the pull with your fingers. Recessed pulls without a handle lip can only be moved sideways, making them ideal for sliding doors. On the other hand, recessed pulls with a handle lip can also be moved forward, making them suitable for hinged doors and drawers.

Rotating Pulls

Read More

Rotating pulls are pulls with a grip that can rotate when in use and be made flat when not in use.
These are recommended for surfaces on which you don’t want to have protruding objects, such as floors and door end surfaces.

Retractable Handles

Read More

Retractable handles (also known as trunk handles) are handles with a movable grip, which can be retracted when not in use.
There is also a type of retractable handle that automatically retracts using spring force.

Push Knobs

Read More

Push knobs have a knob that protrudes when pushed. When not in use, these are safe because the knob component remains flush with the surface of the door and does not stick out.
A selection of push knobs in the same style with a latch mechanism are also available.

For Interior Doors

Interior doors have handles or knobs on both sides as they can be opened from either side. The handles and knobs designed for interior doors are larger and more durable than those intended for furniture.

Door Handles

Read More

Door handles are used for wooden interior doors and glass doors.
A door handle is versatile and can be used for both swinging and sliding doors as it allows for movement in multiple directions, including backward, forward, left, or right.

Lever Handles

Read More

Lever handles are used for wooden interior doors (hinged doors) and glass hinged doors.
They are used with a corresponding case lock (lock case). The latch mechanism is released to open doors when the lever handles are turned.
Our range includes products for use on interior doors.

Pull Handles

Read More

Pull handles are recessed handles used for wooden sliding doors and glass sliding doors.
Pulls are mainly used on sliding doors. They are operated with hooking fingers to slide doors from side to side.

Door Knobs

Read More

Door knobs are knobs used for wooden doors and glass doors.
Door knobs allow for door movement in various directions, including forward, backward, right, and left, making them suitable for swinging and sliding doors.

For Machinery and Equipment

Handles and knobs are commonly used as the opening and closing mechanisms on machines, including sliding doors on machine tools and lids on analysis equipment.
They can be mounted to sheet metal with screws, a quick mounting mechanism, and more.

TB Handle Series

Read More

Our TB Handle series is designed to excel in machine applications, combining durability in various operating environments with a sleek and functional design that we call "beautility."

Learn More

Front Screw Mount Handles

Read More

They are also called "surface mount handles." Surface mount handles are a recommended option when back mounting is not possible due to space constraints or when the handle needs to be mounted in a hard to reach area.

Video: The difference between a back screw mount handle and a front screw mount handle

Back Screw Mount Handles

Read More

Back screw mount handles are installed using screws from the back side of a door.
Without any visible screw heads on the front surface, you can achieve a clean and polished look for your machine or equipment.

Video: The difference between a back screw mount handle and a front screw mount handle

Recessed Pulls

Read More

Recessed pulls are embedded into doors and other equipment.
Large-sized products that can be easily used even with thick industrial gloves are also available.

Retractable Handles

Read More

Retractable handles (also known as trunk handles) are handles with a movable grip, which can be retracted when not in use.
There is also a type of retractable handle that automatically retracts using spring force.

Latch Handles

Read More

Latch handles have a latch mechanism to hold the door closed.
They have a lever or knob that is turned or pushed to engage or disengage the latch.

Knobs

Read More

Handles require a full grip to be operated, while knobs can be operated with just the fingertips.

How to Select the Right Handle, Pull, or Knob

1. Select a Replacement with the Same Mounting Pitch

When replacing a pull or handle, select one with the identical mounting pitch as the previous one to reuse the existing screw holes. The mounting pitch of a pull or handle refers to the measurement between the centers of the mounting holes.

2. Total Design Coordination

Pulls and knobs are available in various designs and styles, including modern, natural, and antique, and using hardware from the same series, such as hooks or a towel rail, can help create a cohesive and visually appealing interior space.

Products for Total Coordination

3. Select SEMI-Compliant Handles for Semiconductor Equipment

SEMI compliance refers to the set of standards created to unify industrial standards worldwide in the semiconductor industry. The SEMI standards specify environmental, health, and safety guidelines, and regulations for handles are also included, so select a handle that complies with these standards.

SEMI-Compliant Handles

Cookies und Datenschutz

Cookies helfen uns, Ihre Webseiten-Erfahrung zu verbessern. Durch die Nutzung unserer Website erklären Sie sich mit der Verwendung von Cookies einverstanden.

Mehr erfahren
You seem to be visiting from Vereinigte Staaten von Amerika. Sugatsune America serves your location.