Zwei L Series

Zwei L
Zwei L logo

CONCEPT

Zwei L

Mirror sparkle resembles the depths of a crystal-clear lake.
Satin as lustrous as the finest spun silk.
The supreme architectural hardware for the convergence of the Zwei Lichter (two lights).
The "Z" stands for ultimate, while the "L" suggests "LAMP" with light - Sugatsune's flagship brand.

TECHNOLOGY

1Exquisite Distortion-free Straight Lines
Zwei L represents the seamless of "two lights" with the utmost precision, achieved through the work of our skilled craftsmen who create exquisitely straight and distortion-free lines.
Our ultimate mirror polishing and silk-like satin finish showcase these straight lines at the boundary of the two lights, bringing out their impeccable beauty.

2Ultimate Mirror Polishing
These high-precision straight lines are handcrafted by skilled polishers, with a level of accuracy that creates an unparalleled mirror-like shine. Our polishing process boasts polishing grain that is twice as fine and has five times the steps of a traditional mirror polish, resulting in a reflective finish that is as clear as the depths of a pristine lake.

3Beautifully Distinct Edges
The beauty of our edges stands out with a sharp impression that maintains its form without any noticeable rounding. Our skilled craftsmen fine-tune the edges to ensure angles that are pleasing to the eye and to the touch.

4Silk-like Satin Finish
Our satin finish is truly remarkable, reflecting a lustrous shine akin to that of high-quality silk. It remains free from any warping, even on curves, and is finished uniformly without any distortion. The finish is so precise that it resembles the perfectly spun thread of silk, creating a truly stunning result.

Zwei L

MATERIAL

All stainless steel (SUS316)
SUS316 is one of the most rust-resistant stainless steels, with excellent corrosion resistance and is used on marine vessels.
All products in the Zwei L series are made from SUS316, which offers excellent durability and will remain beautiful for many years.

Zwei L

Products

60 results

Products per page
25 50 100

60 results