- Furniture and Architectural Hardware
- LAMP Brand
- Stainless Steel Hardware
Stainless Steel Hardware
What is stainless steel?
Stainless steel is an iron-based alloy made with a minimum of 11% of chromium. Further elements such as carbon, nickel, molybdenum or other can also be added in order to improve heat, acid or tensile resistance according to the specific needs. Rust resistance is the best-known property of stainless steel, a result of the chromium combining with oxygen in the air and forming a passivation film on the surface which blocks oxygen ingress. Depending on the composition, it is divided into many types. The following two are some of the most common.
The most common types are SUS303, SUS304 and SUS316. SUS303 contains a small amount of molybdenum in addition to chromium and nickel and offers particularly good scratch resistance. SUS304 has chromium and nickel added, to make it more corrosion resistant and easier to process, making it widely used. SUS316 has chromium and nickel added along with more molybdenum than SUS303. Although it is an expensive material, it offers very good resistance to corrosion.
These types of stainless steel contain very little or no nickel. The most commonly used is SUS430, that although less corrosion resistant than the SUS304 or SUS316, is relatively cheaper. This kind of stainless steel is magnetized.
Chromium (Cr) combines with oxygen in the surrounding environment and forms a passivation film.
Stainless Steel and Humid Climates
Stainless steel is characterized by its resistance to rust, making it an ideal material for homes in humid climates. As stainless steel naturally forms a passivation film to protect against oxygen ingress, it is rust resistant even when scratched.
Mirror-like distortion free surface
At first glance, our mirror finishes immediately appear different. Without distortions, the flat surface has been polished to resemble a mirror. Something only accomplishable with experience and high level techniques. By taking the extra effort to polish to a great deal of precision, the inherent beauty of metal becomes visible to the naked eye.
Satin "ripples" create a silklike texture
Satin finishes visually change depending on the strokes position, length and distance. Our satin finishes are silky fine, and is characterized by a sense of precise uniformity.
High level techniques create lines of light
Different finishes can be incorporated into a single product.
The highest level of polishing skill is evident in the fine, straight lines without distortion.
Products made to last. All stainless steel products.
The large recessed pull is recommended for special industrial and public vehicles and containers. The included screws and nuts are made entirely from stainless steel.
SUS316 and SCS14 products can be used in the marine industry
In the United States, Europe, and other regions where the marine market is thriving, people associate Sugatsune with stainless steel. For cruisers and yachts that are exposed to seawater and sea breezes, even more rust-resistance is required, and we have many products made of SUS316 and SCS14 (equivalent to SUS316) that are ideal for such harsh environments.
Careful edge processing
Outlet plate model PXP-ES (Cool Metal Series) and hotel outlet plate model PXP-ES01M (Cool Metal Series) feature a minimalist design. Because of the simplicity of the design, the finish of the edges determines the design, so we have paid extra attention ensuring the product is safe while still having brilliant edges.
Wide product lineup
A variety of stainless steel products including hinges, hooks, slide rails, and handles are available.
Your Recently Viewed Items
You have no recently viewed products.
If you would like to keep track of items viewed, click on the "Keep History" button below.
You have no recently viewed products.