HES Series Milestones at a Glance

The Evolution of HES Hinges

1989

2022

HES-3030AK
Post-Installation Adjustable

Sugatsune launches one of the first adjustable concealed hinges on the market. The hinge position can be adjusted vertically and horizontally post installation.

1992

HES3D-190
3D Adjustment Feature

The hinge that revolutionised adjustability by introducing the 3D post-installation adjustment feature, adding depth adjustability to the existing vertical and horizontal adjustments.

It also introduced a new feature designed for easier door hanging, dividing into two parts—one for the door side and one for the frame side. Additionally, it includes a temporary hanging feature, allowing you to hold the door in place while mounting it with screws.

2006

HES2S-140-A125
First-Ever Concealed Surface Mount Hinge

The first-ever concealed surface mount hinge, designed to reduce installation time by requiring less mortising. This innovative hinge surface mounts on the door jamb side, making it easier to install and providing a clean, sleek look.

2022

HES1F-140
A Hinge for Flush-to-Wall Doors

A hinge that seamlessly blends into 8 mm frames, creating a flush, almost frameless effect. The slim design ensures a beautifully integrated and sleek appearance, perfectly aligning the door and wall.

2022

HES
SERIES

HES
THROUGH
THE YEARS

  • HES-3030BR

    1989

  • HES-3030AK

    1992

  • HES3D-190

    2006

  • HES3D-160

    2007

  • HES3D-V135LGR

    2010

  • HES3D-120

    2014

    Glass Door Compatible

  • HES3D-E190

    2014

  • HES3D-90

    2015

    Glass Door Compatible

  • HES3D-70

    2016

  • HES3D-E160

    2018

  • HES3D-120-A100

    2019

  • HES3D-W190

    2019

  • HES3D-H120-36

    2020

  • HGS3D-S160SH

    2021

  • HES2S-140-A125

    2022

  • HES1F-140

    2022

  • HES2S-150-A110

    2024

Looking Ahead - The Future of HES Hinges

At Sugatsune, innovation never stops. With each milestone, we’ve pushed the boundaries of what’s possible in hinge technology, setting new standards for quality and design. From the introduction of the HES-3030BR in 1989 to our newest hinge, the HES2S-150-A110 Surface-Mount Concealed Hinge released in 2024, our journey is marked by relentless dedication to excellence.

As we continue to innovate, our commitment remains steadfast: to create products that not only meet but exceed the expectations of our customers. Our latest advancements, including the first-ever concealed surface mount hinge and hinges that seamlessly integrate into slim frames, are just the beginning. At Sugatsune, we are driven by the belief that creating new and innovative products is at the heart of everything we do.

Join us as we look forward to a future where our hinges continue to redefine the industry, providing unparalleled functionality and aesthetics for years to come.

Explore the HES Series

Innovating Hinges for a Better Tomorrow