7 Product Application Images Added Update:2024/04/22

Door in Private Residence

Our HES2S-140-A125 Surface-Mount Concealed Hinge was installed in the door of a private residence.
The HES2S hinge features a unique design that enables surface mounting on the frame side. This capability is made possible by a mechanism that allows the hinge's arm to fold into a socket within the door, concealing the hinge. This innovative design effectively conceals the hinge and enhances the door's aesthetic appeal.
The surface mounting hinge was chosen by the contractor because it simplifies the installation. The design office also appreciated the fact that it could be installed over the wallpaper, which enhanced the design.