7 Product Application Images Added Aggiorna:2023/12/15

Residential

Provided by Sugita Woodworking

[Application Example of Customers]
The slides "4670" were used in the kitchen drawers made by Sugita Woodworking.
The key to the adoption was that it can be used in the size desired by the client and has a soft-close function.

Custom-made kitchen showroom

Provided by MODELLO Corporation Ltd.

The LIN-X1000 (flush sliding door system) was used for the showroom of the custom-made kitchen.
This system is featured in the doors of storage cabinets and aisles. When closed, the doors become flat with the adjacent doors and seamlessly blend into the wall. As the doors open in a small radius, they don't get in the way even when fully opened.

See Related Products