Concealed (European / Cup) Hinges Hardware Basics

Concealed hinges are used for swing doors in various types of furniture and equipment.
On this page, learn the basics about different types of concealed hinges and how to choose them, including some unique options only available from Sugatsune.


What is a concealed hinge?

Concealed hinges, also called cup hinges or European style hinges, are hardware components installed on the interior side of a swing door to enable the door to open and close while also remaining hidden from the outside.

Hidden from view when the door is closed

Can be used for consecutive doors

Easy to attach, detach and adjust

Butt hinges are also used for swing doors, but have three major differences. Firstly, concealed hinges can be installed on the interior of a cabinet. These hinges remain out of sight when the door is closed, contributing to a clean and modern appearance in line with current minimalist design trends.

Unlike traditional butt hinges, concealed hinges have multiple axes, causing the door to follow a distinctive path as it opens, slightly recessing inward. Therefore, it can also be used in places where the wall is very close to it or where doors are lined up consecutively.

Additionally, contemporary concealed hinges feature a simple attachment and detachment mechanism. This design allows for horizontal and vertical adjustments to the door's position even after installation.

Concealed Hinges Components

Main Components:
1. Body
2. Mounting plate

The body is attached to the door, and the mounting plate is attached to the side board of the cabinet.*
Easily attach the door to the cabinet by pushing the bodies into the mounting plates and snapping them in place. Furthermore, lifting the lever on the body will release it from the mounting plate, allowing for the door's detachment.**

*Make sure to choose a combination of body and mounting plate of the same series.
**Only applies to products with the simple attach/detach mechanism.

Video: OLYMPIA CONCEALED HINGE Attach/Detach

Types of Concealed Hinges

Door Material

Wooden Doors

When installing on wood, standard concealed hinges are used.

Glass Doors

The optional face plate allows for installation on glass doors. Some OLYMPIA/J95 series hinges are compatible with the glass face plate.

Sheet Metal Doors

Concealed hinges can also be used on sheet metal.

Door Overlay

The overlay refers to the area where the side panel and door overlap.
Overlays can be divided into the following three types.

(1)Side panel (2)Door

Full Overlay

A full overlay door covers the entire face frame of cabinets.
The side panels are almost invisible when viewed from the front, allowing for a sleek design.

(1)Side panel (2)Door

Inset

An inset door is precisely fitted inside the side panels of cabinets.
Because inset doors have the ability to close at an angle greater than 90°, as they do not make contact with the side panels, it is advisable to install a door stop to prevent the door from over-closing inward.

(1)Side panel (2)Door

Half Overlay

A half overlay cabinet door partially covers a portion of the side panels.
Half overlays are recommended for consecutive doors. As shown above, when the closing door makes contact with the side panel, it stops, eliminating the need for a door stop.



"Overlay 15~19mm (When Bore Distance is 5mm)" in our catalogue refers to the conditions shown. The "15-19mm" specification indicates that the overlay can be reduced up to -4mm with the adjustment screw.
Bore Distance refers to the distance from the edge of the door to the cup hole. The 5mm Bore Distance indicates the measurement from the door's edge to the beginning of the hinge mortise. If this distance is less than 5mm, it causes the door to move to the left, leading to a reduction in overlay and revealing part of the side panel. You can find the relevant bore distances listed in the catalogue for your convenience. Please refer to our catalogues for applicable Bore Distances.


Details of cup diameters and bore depths

Opening Angles

90°- 105° Opening

Standard opening angles.

85° Opening

An 85-degree door opening is recommended when walls or objects are in close proximity to the fully opened door. Standard door opening angles could lead to the door or knob making contact with these structures.
Some products with standard opening angles can be adjusted to 85° opening with additional parts.

140°-160° Opening
(Wide Angles)

At wide angles, the door doesn't get in the way when items are taken in and out of storage.

Door Mechanisms

The way a door moves varies depending on the type of concealed hinge used. There are four primary types of motion.

Soft Close: With Built-In Damper

The soft close mechanism enables doors to close slowly and quietly. It prevents sudden slamming and creates a sense of refinement to their movement.
For soft close, select concealed hinges with a built-in damper. Some types also allow for speed adjustment.
For a single door, usually two or more concealed hinges are required. However, if all of these hinges have dampers, it could result in the door closing too slowly. Certain products offer recommendations regarding the optimal number of hinges with dampers to use. Please use these recommendations as a reference.

Push Open

The push open concealed hinge features a built-in spring that has force in the opening direction.
Combine it with a touch latch to create a push-to-open door. Due to the door's push-to-open mechanism, there is no need for knobs or handles.

Prevents Unintentional Door Opening
(With Catch)

A concealed hinge with catch has a built-in spring. The spring pulls the door inward, so the door closes automatically at a certain angle. Additionally, it can assist in firmly keeping the door closed and reducing the chances of unintentional door opening.
If all concealed hinges on a single door are equipped with catches, the closing force of the door will be too strong. Combining hinges without catches and hinges with catches results in a gentler door-closing force.

Free-Swing Opening
(Without Catch)

A concealed hinge without a catch does not have a spring. The door does not close automatically and is not securely kept closed. Use a concealed hinge with a catch or add a separate magnetic catch to firmly keep the door in a closed position.

Colour Variations

Silver

Silver is the standard colour for concealed hinges.

Black

Black options are available for certain concealed hinges and mounting plates.
Choose the hinge hardware to match the colour of the furniture it will be mounted on.

How to Choose Concealed Hinge Hardware

STEP 1: Select a concealed hinge


Please refer to "Types of Concealed Hinges" to choose a concealed hinge.
Use our website's filter to easily find concealed hinges that match your desired specifications by checking boxes like "Opening Angle," "Overlay Range," etc.

The number of concealed hinges per door varies based on the door's size and weight.



STEP 2: Select a mounting plate


Please select a mounting plate from the same series as the concealed hinge.

Three types are available for some series: Plates with 2, 3, or 4 screw holes.
Mounting plates with two screw holes have a slim and sleek appearance. The difference between the three-hole and four-hole types is in their mounting strength. Please choose four-hole types for large or heavy doors.

Mounting plates with a thickness of +2mm or +5mm are available in some series and can be used to reduce the overlay.
Please refer to How to Adjust the Door Position for details.


STEP 3: Select optional items as required


Sugatsune provides optional items like covers to conceal the adjusting/mounting screws and angle limiters to set the door's opening angle to around 85°.
Please select an optional item from the same series as the concealed hinge main body chosen in STEP1.

Design Considerations


When designing furniture with concealed hinges, the Opening Clearance (O.C) must be considered. Opening clearance (O.C) is the space required when opening and closing doors. It is very important because if it is not secured, the door will collide and not open.

Please refer to the locus chart on the right. In the closed position and while the door is being opened, the position of the edge of the hinge stile (where the concealed hinges are attached) varies. When the door is in the process of opening, it sticks out more than when it's fully closed. In other words, to prevent the door from hitting anything when the edge of the hinge stile protrudes the most during its movement, it's crucial to maintain some clearance on the side where the hinges are located.

Opening Clearance (B)

Opening clearance is also needed for the leading door edge side.

Clearance for
Door Edge O.C. (A)


The opening clearance varies depending on the door thickness and the Bore Distance. For example, in case of an outset door as shown in the diagram, if the door thickness is 20mm and the Bore Distance is 5mm, the required opening clearance is 1.8mm. This table can be found on the concealed hinge pages within the catalogue. Please consult this information when designing a door that incorporates concealed hinges.

Door Processing: Cup Diameter and Bore Depth

To mount the main body of the concealed hinge on the door, create holes similar to the ones shown in the picture. The diameter and depth of the hole are determined by the diameter (cup diameter) and depth (bore depth) of the concealed hinge cup. Find the detailed processing dimensions on each product page in the catalogue.

How to Adjust Door Position

Most concealed hinges come with 3D adjustability (Vertical/Horizontal/Depth). Hinges can be adjusted post installation, simply by turning the adjustment screw with a screwdriver.

Other Methods to Adjust Overlay



Adjusting Overlay with a Distance Plate

By inserting distance plate(s) under the mounting plate as shown in the diagram, the amount of overlay can be reduced by the thickness of the plate. For example, if you insert one 2mm thick distance plate, the overlay will decrease by 2mm, and if you use two, it will decrease by 4mm.

Adjusting Overlay with a Thicker Mounting Plate

The function of mounting plates are very similar to distance plates. By changing to a thicker mounting plate, the overlay can be reduced. For example, when you switch from the standard thickness plate to one that is +5mm thicker, the overlay will decrease by 5mm.

Concealed Hinge Series

OLYMPIA 360 Series

Select from five different settings to modify the soft-close force. While JIS (Japanese Standards) mandates 40,000 cycles, OLYMPIA has exceeded this requirement by undergoing 200,000 cycles to ensure outstanding durability.

J95 Series

The J95 series is designed for heavy-duty applications, making it suitable for large and heavy doors. Just two J95 hinges can replace the need for five conventional hinges. Not only does create a clean aesthetic, but it also reduces installation time.

J160 Series

The J160 is a wide-angle heavy-duty concealed hinge. This hinge enables doors to open up to 160°, ensuring the doors remain out of the way when accessing the inside of cabinets or other storage furniture. It also a features a soft-close function.

Stainless Steel 100 Series

All concealed hinges in the 100 series are made of stainless steel. Due to its excellent corrosion resistance, it is recommended for kitchen equipment and marine vessels.

Privacidad y cookies

Las cookies nos ayudan a mejorar su experiencia en el sitio web. Al utilizar nuestro sitio web, acepta nuestro uso de cookies.

Saber más