Clean Food Equipment Even More Efficiently!

Assist Torque Hinges Help Reduce the Workload

Higuchi Co., Ltd. have adopted the HG-TLAJ-40 Spring-Assist Torque Hinge for their food machinery (dry automatic peeling devices).

PROBLEM

Key Issues

  1. Previously, the lids had to be removed to clean the devices, which was time-consuming and extended the overall cleaning time.

Product Information

Spring-Assist Torque Hinge / HG-TLAJ

  • Spring assist makes it easy to open lids and covers.
  • Assist range of 100°.
  • Retaining torque can be adjusted (0 to 3.5 N·m) by turning the adjustment screw (nominal 10 spanner).
  • Plastic cover (sold separately) covers the hinge and mounting holes for a cleaner look.

*Information as of 20th August 2024.

SOLUTION

The Solution

  1. The HG-TLAJ Spring Assist Torque Hinges allow the lids to be easily lifted and held in place, eliminating the need to remove them for cleaning and reducing the overall cleaning time.
  2. They also prevent accidental closure, minimising the risk of injuries.

Appearance after installation

Customer Feedback

  • Please tell us why you chose the HG-TLAJ hinge.
    We adopted the hinges with the aim of making cleaning easier, and reducing cleaning time, after using the devices.
    Previously, the lids had to be removed to wash the devices, but with the spring-assist torque hinges, the devices can now be rinsed simply by lifting the lids, without removing them.
  • How has the HG-TLAJ hinge performed after adoption?
    We have been able to reduce our cleaning times.
    We feel that the benefits of this system include the ability to open the lids with ease, since food processing sites are often staffed by women, and the fact that the lids do not close unexpectedly, which helps prevent injuries.
  • Please let us know if you have any requests for the future.
    We would appreciate any suggestions you could give us for products that would help reduce costs and improve functionality.

Sales Manager:
Thank you for choosing our product and providing valuable feedback.
We will continue to propose products that are beneficial to you.