Build a Safe and Easy-to-Use Workbench: A Lift-Up Work Table

Our lift-assist dampers LAD have been adopted for the lift-up work tables used by Yamakin Industry Corporate in their logistics sites.

PROBLEM

Key Issues

  1. Crossing over conveyors in shipping and packaging lines required either using a crossover ladder, which posed a risk of workers falling, or lifting a section of the conveyor to pass through.
  2. Additionally, the lift-up section also posed a risk of falling and causing injuries to the hands if it fell unexpectedly.

Product Information

LIFT-ASSIST DAMPER LAD

— Tabletops close gently and quietly. Soft-closing even at slight opening angles.
— Lift-assist feature allows tabletops to be lifted easily.
— Can be retrofitted to existing tabletops with no modifications.

*Information as of 15 December 2023.

SOLUTION

The Solution

  1. Lifting the table's flap allows safe passage without the need to cross over the conveyor, improving convenience and eliminating the risk of falling.
  2. Introduced lift-assist dampers to create a slow-closing, lift-up work table, significantly reducing the risk of hand injuries.

The LAD lift-assist dampers are installed onto the lift-up tabletop section. These dampers are equipped with a lift-assist feature, allowing the tabletop to be lifted with minimal effort. Additionally, the tabletop closes slowly and quietly (soft-closing) to reduce finger pinching.

Image in use: During operation, packages slide in from the conveyor belt, and during breaks, the tabletop can be flipped up to allow easy passage.

This product contributes to safety measures at logistics sites. See it in action in the video below. The tabletop can be lifted smoothly and closed gently.

Another key feature is the slim profile of the arm unit. When opened, it only sticks out by 35mm, meaning it won't obstruct any passageways.

Yamakin Industry Corporate's work tables have solved safety issues on shipping and packaging lines, such as the risk of hands getting caught when passing through a lift-up conveyor belt if it falls, and the risk of falling when stepping over a conveyor using a step.
LAD lift-assist dampers can be used not only in logistics sites, but also around counters in stores and other locations.

Filming cooperation, provision of photos
Yamakin Industry Corporate