Key Issues
- Black hinge and lock hardware was needed to coordinate with a chic black store interior.
Product Information
GS-G Series GLASS HINGE / GS-GH20
— Hinges for inset glass showcase doors.
— The design can be coordinated by using it together with the GLASS BRACKET GS-GB20 and the GLASS DOOR LOCK GS-GL20.
— The temporary fixing function makes it easy for one person to install.
— By turning the adjustment screw, the door can be adjusted to the left or right post-installation.
*Information as of 6 September 2021.
GS-G Series GLASS DOOR LOCK / GS-GL20
— The design can be coordinated by using it together with the GLASS BRACKET GS-GB20 and the GLASS HINGE GS-GH20.
— The included door stopper helps make locking the door easier.
*Information as of 6 September 2021.
Million Lock Series CABINET LOCK / 7810
— Dimple key type. Key is reversible so it can be inserted easily.
— The same key can be used with multiple locks if the same key number is specified.
*Information as of 6 September 2021.
The Solution
- The black GS-G series glass showcase hardware was selected to create the desired stylish aesthetic for the shop showcases.
- Using the Total Lock Series, one key conveniently opens glass showcases and storage drawers that are set to the same key number.
Black hardware to match all black furnishings to create a stylish space.
The client wanted to create a classy movie shop with all-black walls and store furnishings. They also wanted matching black showcase hinges and locks.
With the sleek black color and muted finish, the GS-G series glass showcase hardware enabled the hinges and locks to be coordinated with the furniture. The hardware also enhanced the sharp and flat look creating stylish showcases.
Manage multiple locks with one key on glass and wood
The black Million Lock surface-mounted cylinder lock 7810 was installed in the storage drawer located beneath the glass showcase. It was set to the same key number as the matching cylinder glass lock GS-GL20 used in the showcase. This is one of the key features of the GS-G series, as it offers versatility and can be applied to both wood and glass hardware.
As the same key can be used to unlock the showcase door and the stock drawer, merchandise can easily be moved around.
*The same key number must be specified within the same series in order to unlock with a single key.