Sugatsune Hardware Ideas for Residential Spaces

Living space suggestions using Sugatsune hardware

A home that can satisfy each and every client.
For all the contractors who are uncompromising about building homes such as these, Sugatsune offers suggestions for fittings that utilise its hardware.
For example: kitchen storage focused on ease of use. Hotel-like bathroom interiors. Living spaces where you can fully enjoy your "me time".
Sugatsune hardware helps to create spaces that bring joy to our customers, in response to all their ideas and needs.

  • Living Room
  • Kitchen
  • Bedroom
  • Bathroom
  • Entryway

Organize the flow of household chores, for personalised convenience

Adding a little ingenuity to our fittings means we can offer you the ideal kitchen, combining looks and practicality.

Examples of specialist kitchen fittings

Keep waste baskets or signs of wear out of sight

In areas such as the bathroom, lavatory and kitchen, where signs of wear are more obvious, concealed storage of the kind you would find in a store can be incorporated to create a hotel-like feel.

TRASH GROMMETS (MULTI-PURPOSE LIDS)

Parallel sliding doors that can be fully opened even in narrow spaces

By using a door fitting with a specialised trajectory that will not impede the flow of motion, you can make good use of narrow spaces such as kitchen corners or bathroom storage.

MONOFLAT LIN-X HINGE
LIN-X450

Expand your workspace with a folding table

Not enough workspace? Solve the problem with a folding shelf bracket. Includes built-in damper for foolproof fall prevention.

FOLDING BRACKET
388-D

Multi-purpose use of space

Our ingenuity in accommodating your lifestyle will help you live the life that suits you.

Examples of specialist fittings for bedrooms and living rooms

Parallel sliding doors that can be fully opened to choose clothes easily

Specialised trajectory allows for wide-opening storage even in narrow spaces such as hallways. Can be opened and closed in about half the space of a conventional swing door.

MONOFLAT LIN-X HINGE
LIN-X800

Folding workspace for a more spacious feel

Folding shelf bracket with built-in damper. Depending on the options, the bracket can be operated with one hand up to a maximum width of 3 metres.

FOLDING BRACKET EBN-DA

Conceal signs of wear while maintaining practicality

Especially when space is limited, these fittings are particularly effective at providing you a convenient and stress-free lifestyle.

Examples of specialist bathroom fittings

Layout freedom to meet your storage needs

We offer a wide range of four-post shelf supports that allow you to set up your shelves at any height.
We also offer optional items with added features that can give you peace of mind.

STAINLESS STEEL SHELF STANDARD
SP, SPS

Coordinate your walls with a unified design

Urban design to suit minimalist tastes. Its big feature is the beautiful detailing, suitable for specialised interiors.

Urban Metal Series

Storage doors that do not block the flow of movement even when left open

Want to hide signs of wear without sacrificing everyday convenience? Our POCKET DOOR SYSTEMS hardware provides you with convenient hidden storage.

POCKET DOOR SYSTEMS

Attractive display storage and discreet hidden storage for increased satisfaction

Even cluttered spaces can be neatly organized with a little ingenuity in the fittings.

Examples of specialist entryway fittings

Concealed door to hide mudroom storage seamlessly within the wall

These sliding door fittings can be used to create hidden rooms. The doors seamlessly blend with the walls, giving you the storage you want in entryways, living rooms, or other clutter-prone spaces.

FLUSH SLIDING DOOR SYSTEM
MFU1200

Keep pet leads on a hook that they won’t easily come off of

This ring-shaped latch hook prevents items hung on it from falling off easily.
Ideal for hanging up pet leads, as well as for storing tools in entryways, garages, and so on.

LATCH HOOK
EN-R80

Comprehensive Support Content

A showcase of problem solving examples!

We regularly post case studies where problems have been solved using Sugatsune products on our website. Please feel free to use these for inspiration.

Conventional Stay

Gets in the way…

Gets in the way…

Mounted at 3 points

Aileron

Compact!

Compact!

Mounted at 2 points

Build Better with Sugatsune!

Sugatsune provides innovative hardware solutions for designers, builders and manufacturers, and also offers extensive support to its customers. At the Sugatsune Help Hub, we combine digital technology with on-site expertise to provide consistent support from the concept stage through to completion. You can rely on us to bring your ideas to life, and to help make sure your projects progress smoothly.