16 Product Application Images Added Update:2023/09/07

Built-in TV Wall Unit
Built-in TV Wall Unit

Our soft-down stays and drop hinges were utilised in a custom-built built-in TV wall unit. The sleek black face plates seamlessly integrate with the tinted glass doors. On the back side of the wall, there is a spacious storage area that also functions as a wiring space for wall-mounted TVs, as well as a charging dock for a robot vacuum cleaner. This smart and integrated design enhances the overall organization and clean style of the living room.
*This application example has been provided by one of our customers, who has granted permission for its use.

#builtinwallfurniture #spacesavingstorage #spaceforrobotvacuum #cleanaesthetic #cleandesign #builtinfurnituresolutions #builtinfurniture

Example of using in a shelf standard horizontally

Bathroom

For sliding doors in residential and hotel bathrooms.

Stainless steel is used for parts for corrosion resistance.
The maximum door width is 1200mm, allowing wheelchairs to pass smoothly.

Private Booth
Private Booth

For private office booths.
Up to 27 kg lightweight doors can be surface-mounted on the upper roller. This makes it ideal for sliding aluminum frame doors with plastic panels.

#teleworkbooth #workbooth

Storage Bench
Storage Bench

Our Ailreon stay received positive feedback for the clean design achieved by back panel mounting and the easy installation due to the integrated design with concealed hinges.

See Related Products
Educational Dining Table for Children
Educational Dining Table for Children

Our concealed hinge "OLYMPIA" was adopted for the doors of children's educational dining tables.

See Related Products
Future-Concept Kitchen
Future-Concept Kitchen

Our multi-purpose lid was incorporated into a future-concept kitchen.
The touchless and automatic-opening lid was integrated into the trash bin under the sink.